REGEN.UTFTHRESH

Description

This parameter returns the over temperature warning threshold of the power circuit for the regen resistor. The value depends on the drive model. It is programmed in the drive and cannot be changed.

Versions

Action

Version

Notes

Implemented

02-08-01-000

General Information

Type

Read Only

Units

Deg C

Range

N/A

Default Value

N/A

Data Type

Float
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
REGEN.UTFTHRESH

3007h

0eh

Signed32

-

-

Read only

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

REGEN.UTFTHRESH

2413

96D

Signed32

Read Only

-

PROFINET

Parameter

PNU

Data Type

Access

Units

REGEN.UTFTHRESH

2413

Float

Read Only

-